JAJSGA2F September 2018 – June 2021 TPS2663
PRODUCTION DATA
The TPS2663x devices feature an accurate ± 2% adjustable undervoltage lockout functionality. When the voltage at UVLO pin falls below V(UVLOF) during input undervoltage fault, the internal FET quickly turns off and FLT is asserted. The UVLO comparator has a hysteresis of 78 mV (typical). To set the input UVLO threshold, connect a resistor divider network from IN supply to UVLO terminal to GND as shown in the Simplified Schematic. The TPS2663x devices also features a factory set 15-V input supply undervoltage lockout V(IN_SYS_UVLO) threshold with 1-V hysteresis. This feature can be enabled by connecting the UVLO terminal directly to the GND terminal. If the Undervoltage Lock-Out function is not needed, the UVLO terminal must be connected to the IN_SYS terminal. UVLO terminal must not be left floating. In the applications where reverse polarity protection is required connect a minimum of 300-kΩ resistor between UVLO and IN_SYS.
Figure 8-1 shows the turn ON behavior when UVLO pin voltage exceeds V(UVLOR) threshold.