JAJSKH0C April 2023 – February 2024 TPS274C65
PRODUCTION DATA
The ground connection may be lost either on the device level or on the module level. If the ground connection is lost, both the channel outputs will be disabled irrespective of the EN input level. If the switch was already disabled when the ground connection was lost, the outputs will remain disabled even when the channels are enabled. The steady state current from the output to the load that remains connected to the system ground is below the level specified in the Specifications section of this document. When the ground is reconnected, normal operation will resume.