DLPU124 june   2023

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. Overview
  5. If You Need Assistance
  6. DLP LightCrafter DLPC910 EVM (DLPLCRC910EVM) Overview
    1. 3.1  Welcome
    2. 3.2  DLP LightCrafter DLPC910 Evaluation Module (DLPLCRC910EVM) Hardware
    3. 3.3  DLPLCRC910EVM Board
    4. 3.4  Other Items Needed for Operation
    5. 3.5  DLPLCRC910EVM Connections
    6. 3.6  DLP LightCrafter DLPC910 LEDs
    7. 3.7  Apps FPGA Trigger Input
    8. 3.8  DLPLCRC910EVM HPC FMC Cables
    9. 3.9  DLPLCRC910EVM and DMD EVM Assembly
    10. 3.10 Connecting an Apps FPGA Board to the DLPLCRC910EVM
  7. Quick Start
    1. 4.1 Power-up the DLPLCRC910EVM
    2. 4.2 Power-down the DLPLCRC910EVM
  8. Operating the DLPLCRC910EVM
    1. 5.1 DLPLCRC910EVM GUI and Apps FPGA Software
    2. 5.2 PC Software
      1. 5.2.1 Menu Bar
      2. 5.2.2 Icon Bar
      3. 5.2.3 Main Window
        1. 5.2.3.1 Script Commands sub-window
          1. 5.2.3.1.1 Load Tab
          2. 5.2.3.1.2 Reset Tab
          3. 5.2.3.1.3 Clear Tab
          4. 5.2.3.1.4 Float Tab
          5. 5.2.3.1.5 Control Tab
        2. 5.2.3.2 Script Sub-Window
        3. 5.2.3.3 Status Sub-Window
      4. 5.2.4 DLPC910 Registers
        1. 5.2.4.1 Status/Control Tab
          1. 5.2.4.1.1 Status Items
          2. 5.2.4.1.2 DMD Control Items
          3. 5.2.4.1.3 Design Items
        2. 5.2.4.2 Register List Tab
          1. 5.2.4.2.1  DESTOP_INTERRUPT_CLEAR - 0x0000
          2. 5.2.4.2.2  DESTOP_INTERRUPT_SET - 0x0004
          3. 5.2.4.2.3  DESTOP_INTERRUPT_ENABLE - 0x0008
          4. 5.2.4.2.4  MAIN_STATUS (DLPC910) - 0x000C
          5. 5.2.4.2.5  DESTOP_CAL - 0x0010
          6. 5.2.4.2.6  DESTOP_DMD_ID_REG - 0x0014
          7. 5.2.4.2.7  DESTOP_CATBITS_REG - 0x0018
          8. 5.2.4.2.8  DESTOP_910VERSION_REG - 0x001C
          9. 5.2.4.2.9  DESTOP_RESET_REG - 0x0020
          10. 5.2.4.2.10 DESTOP_INFIFO_STATUS - 0x0024
          11. 5.2.4.2.11 DESTOP_BUS_SWAP - 0x0028
          12. 5.2.4.2.12 DESTOP_DMDCTRL - 0x002C
          13. 5.2.4.2.13 DESTOP_BIT_FLIP - 0x0030
        3. 5.2.4.3 Settings Tab
      5. 5.2.5 Apps FPGA Registers
        1. 5.2.5.1 Status/Control Tab
          1. 5.2.5.1.1 Status Items
          2. 5.2.5.1.2 PBC Control Items
          3. 5.2.5.1.3 Row/Block Operations Items
          4. 5.2.5.1.4 Test Pattern Items
        2. 5.2.5.2 Apps Registers Tab
          1. 5.2.5.2.1  APPS_INTERRUPT_CLEAR - 0x0000
          2. 5.2.5.2.2  APPS_INTERRUPT_SET - 0x0004
          3. 5.2.5.2.3  APPS_INTERRUPT_ENABLE - 0x0008
          4. 5.2.5.2.4  MAIN_STATUS (Apps) - 0x000C
          5. 5.2.5.2.5  APPS_CNTRL - 0x0010
          6. 5.2.5.2.6  APPSTOP_PATTERNSEL - 0x0014
          7. 5.2.5.2.7  APPSTOP_TEST_ROWADDR - 0x0018
          8. 5.2.5.2.8  APPSTOP_LOADER_RESET_TYPE - 0x001C
          9. 5.2.5.2.9  DMD_TYPEREG - 0x0020
          10. 5.2.5.2.10 APPS_BUFFER_WSTART - 0x0024
          11. 5.2.5.2.11 APPS_FIFO_BURST - 0x0028
          12. 5.2.5.2.12 APPS_ROW_CTRL - 0x002C
          13. 5.2.5.2.13 APPS_BLK_CTRL - 0x0030
          14. 5.2.5.2.14 APPS_ROW_LOADER - 0x0034
          15. 5.2.5.2.15 APPS_LOAD_TRIG_INTERVAL - 0x0038
          16. 5.2.5.2.16 APPS_EXPOSE_TIME - 0x003C
          17. 5.2.5.2.17 APPS_LOADER_CTRL - 0x0040
          18. 5.2.5.2.18 APPS_DMD_PARK - 0x0044
          19. 5.2.5.2.19 APPS_EXT_RST_EVT - 0x0048
          20. 5.2.5.2.20 APPS_BUILD_DATE - 0x0080
          21. 5.2.5.2.21 APPS_VERSION - 0x0084
          22. 5.2.5.2.22 APPS_FIXED_ID - 0x0088
          23. 5.2.5.2.23 APPS_GPIF_TEST - 0x008C
    3. 5.3 JTAG Flash Programming
    4. 5.4 SPI Flash Programming
    5. 5.5 AMD Xilinx VC-707 Configuration PROM Programming
    6. 5.6 USB Firmware Programming
  9. Connectors
    1. 6.1  J1 - USB - Micro B USB 2.0 Connector
    2. 6.2  J2 - DLPC910 I2C Connector
    3. 6.3  J4 - PMBUS (I2C) Connector
    4. 6.4  J6 - USB GPIO Connector
    5. 6.5  J8 - 400 Position FMC Connector (Female)
    6. 6.6  J14 - Power (Alternate)
    7. 6.7  J15 - Power
    8. 6.8  J17 - JTAG Boundary Scan Connector
    9. 6.9  J18 - SPI Programming Connector
    10. 6.10 J19, J20, and J21 - Fan Connectors
    11. 6.11 J500, J501 - FMC Connector (Male)
  10. DLPLCRC910EVM Power Supply Requirements
    1. 7.1 External Power Supply Requirements
  11. Related Documentation from Texas Instruments
  12. Abbreviations and Acronyms
  13. 10Safety
    1. 10.1 Caution Labels
Row/Block Operations Items
GUID-20230423-SS0I-6MSS-0TTV-GXFPTV1B8LKT-low.svg Figure 5-24 Row/Block Operations
  • Row Operation
    Note:
    • The DLP6500FLQ has 1080 addressable rows (0 - 1079)
    • The DLP9000X and DLP9000XUV have 1600 addressable rows (0 - 1599)
    Addressing any row beyond these limits is ignored.
    • No-op radio button - sends a row command with no row operation
    • Increment radio button - starting at the current row pointer address, increments the DMD row pointer and loads the data to that row. If Number of Rows is specified loads the number of rows specified.
    • Set row: radio button - Sets the row address pointer specified by the Row address entry box and loads the data to the row. If Number of Rows is specified loads the number of rows specified starting at the row specified by Set row.
      • Row address entry box - specifies the starting row address for Set row
    • Zero row radio button - sends the row address pointer to the beginning row of the DMD. If Flip top and bottom is active, sends the row address pointer to the bottom row of the DMD.
    • Number of Rows: entry box - specifies the number of rows to load for Increment, and Set row.
    • Rows all on checkbox - When checked all "ones" are sent to the rows operated on by the commands in the Row operation group.

    Once the desired parameters are set press the Set button to send the operation to the Apps FPGA for execution.

  • Block Operation
    • No-op radio button - sends a row command with no block operation
    • Clear radio button
      • Dropdown selection box - selects the DMD block to clear (load "zeros"):
        • The DLP9000X DMD and DLP9000XUV DMD have 16 selectable blocks
        • The DLP6500 DMD has 15 selectable blocks
    • Reset Single: radio button
      • Dropdown selection box - selects the DMD block to perform a single block reset on:
        • The DLP9000X DMD and DLP9000XUV have 16 selectable blocks
        • The DLP6500 DMD has 15 selectable blocks
    • Reset Dual: radio button
      • Dropdown selection box - selects the DMD block group to perform a dual block reset on:
        • The DLP9000X DMD and DLP9000XUV have the following selectable dual block groups - (1,2), (3,4), (5,6), (7,8), (9,10), (11,12), (13,14), and (15,16).
        • The DLP6500 DMD has the following selectable dual block groups - (1,2), (3,4), (5,6), (7,8), (9,10), (11,12), (13,14), and (15).
    • Reset Quad: radio button
      • Dropdown selection box - selects the DMD block group to perform a quad block reset on:
        • The DLP9000X DMD and DLP9000XUV have the following selectable quad block groups - (1-4), (5-8), (9-12), and (13-16)
        • The DLP6500 DMD has the following selectable quad block groups - (1-4), (5-8), (9-12), and (13-15)
    • Reset Global radio button - sends a reset to all blocks on the DMD at the same time.
    • Mirror Float radio button - sends a specialized reset waveform to the DMD mirrors to release the mirrors and leave them nominally flat.
      Note: Mirror Float is NOT a substitute for a DMD Park (PWR_FLOAT) when preparing to shut down the system.

    Once the desired parameters are set press the Set button to send the operation to the Apps FPGA for execution.