The DLPC910 SPI Flash HEX file to use in this procedure is found here: DLPR910
- To program the DLPC910 controller code
into the attached SPI Flash memory via a SPI programmer the following resistors need to be
temporarily removed to program the SPI Flash memory:
Note: A suggested method to
remove these resistors is to
solder them to the pad at one end or the other so that the resistors are not in the
circuit, but do not get lost.
- Connect a SPI programming cable to the
SPI Programming Connector J18
- Power up the DLPLCRC910EVM board and
program the SPI Flash memory with the *.hex file using your programming software:
- Select the S25FL032 SPI Flash Device
in your programming software
- Select the *.hex file in your
programming software
- Program and verify the SPI
program
- Power down the DLPLCRC910EVM and replace the resistors removed from the circuit in step
1.
- Power up the board and verify that the board is configuring and working correctly.