JAJSDF8B March 2017 – July 2019 LMK04616
PRODUCTION DATA.
This mode allows an external source to SYNChronously turn on or off a continuous stream of SYSREF pulses using the SYNC pin.
When programming EN_SYNC_PIN_FUNC= 1, SYNC_PIN_FUNC=01 and OUTCH_SYSREF_PLSCNT=0, the SYSREF output is in pin mode. The SYSREF pulses can be controlled by the pulse width at the SYNC pin. When the SYNC pin is asserted, the channel is SYNChronously set to continuous mode providing continuous pulses at the SYSREF frequency until the SYNC pin is unasserted. SYSREF stops after completing the final pulse SYNChronously.
Figure 47. SYSREF Request