SBAU378A September 2021 – January 2022 ADS1148 , ADS1248
Although the ADS1x48EVM is designed for measuring all types of analog temperature sensors, general-purpose input signals can be applied to the ADS1x48 through the TC± inputs on the J5 terminal block. Figure 3-21 shows the input structure used for the TC± inputs.
Figure 3-21 Using the TC± Inputs on J5 as General-Purpose Signal InputsAs Figure 3-21 shows, resistors R24 and R23 are not populated by default, resulting in a set of analog inputs that are only subject to the differential filter cutoff frequency of 1.93 kHz and the common-mode filter cutoff frequency of 38.63 kHz. The TC± inputs can therefore be used for any general input signal as long as the ADS1x48 absolute input and common-mode range requirements are satisfied. Select the AIN4 and AIN5 inputs on the ADS1x48 to measure a voltage connected to the TC± inputs.