SLAAE72 December 2022 MSPM0L1105 , MSPM0L1106 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
PD0 and PD1 power supply is automatically controlled by SYSCTL according to the power mode setting. Users do not need to control the power supply manually.
When PD1 peripherals are forced to a disabled state by SYSCTL upon entry into a STOP or STANDBY mode, most PD1 peripheral configuration settings are retained. See the peripheral-specific chapter in the TRM for details on which peripheral registers are retained.
If a PD1 peripheral was multiplexed to an IO pin (through the IOMUX) in an output configuration, the last valid IO output state is latched upon entry to STOP or STANDBY mode. This feature can be a leakage current source.