SLUAAH0 February   2022 UCC14130-Q1 , UCC14131-Q1 , UCC14140-Q1 , UCC14141-Q1 , UCC14240-Q1 , UCC14241-Q1 , UCC14340-Q1 , UCC14341-Q1 , UCC15240-Q1 , UCC15241-Q1

 

  1.   Trademarks
  2. Introduction
    1. 1.1 Pin Configuration and Functions
  3. Three-Phase Traction Inverter
  4. Gate Drive Bias Requirements
    1. 3.1 Gate Drive Bias Architectures
    2. 3.2 IGBT vs. SiC
    3. 3.3 Determining Required Bias Supply Power
    4. 3.4 Input Voltage Requirements
    5. 3.5 Output Voltage Requirements
  5. Single Positive Isolated Output Voltage
  6. Dual Positive and Negative Output Voltages
  7. Dual Positive Output Voltages
  8. Capacitor Selection
  9. RLIM Current Limit Resistor
    1. 8.1 RLIM Functional Description
    2. 8.2 RLIM Dual Output Configuration
      1. 8.2.1 CVEE Above Nominal Value CVDD Below Nominal Value
      2. 8.2.2 CVEE Below Nominal Value CVDD Above Nominal Value
      3. 8.2.3 Gate Driver Quiescent Current: IQ_VEE > IQ_VDD
      4. 8.2.4 Gate Driver Quiescent Current: IQ_VEE < IQ_VDD
      5. 8.2.5 CVEE Above Nominal Value CVDD Below Nominal Value: IQ_VEE > IQ_VDD
      6. 8.2.6 CVEE Below Nominal Value CVDD Above Nominal Value: IQ_VEE < IQ_VDD
    3. 8.3 RLIM Single Output Configuration
  10. UCC14240-Q1 Excel Design Calculator Tool
  11. 10Thermal Considerations
    1. 10.1 Thermal Resistance
    2. 10.2 Junction-to-Top Thermal Characterization Parameter
    3. 10.3 Thermal Measurement and TJ Calculation Example
  12. 11Enable (ENA) and Power Good (/PG)
  13. 12PCB Layout Considerations
  14. 13Reference Design Example
  15. 14Summary
  16. 15References

Thermal Measurement and TJ Calculation Example

For the UCC14240-Q1 used in an EVM operating at VIN=24 V, VDD-VEE=20 V and POUT=1.62 W with η=57%, the power dissipation is determined as:

Equation 40. PD=POUT×1η-1=1.62 W×10.57-1=1.22 W

The maximum case temperature is measured as TC=61°C at TA=26°C ambient and the resulting thermal image is shown in Figure 10-1.


GUID-20220126-SS0I-QBTS-91VR-37PDTBXMPSWB-low.png

Figure 10-1 UCC14240-Q1 Max Case Temperature, POUT=1.62 W

Using the ΨJT thermal metric that was derived from the EVM closely representing how the UCC14240-Q1 PCB is expected to be designed, we obtain a TJ of 81.25°C as shown in Equation 41. Applying ΨJT is therefore considered the most accurate method for estimating TJ.

Equation 41. TJ=TC+ΨJT×PD=61+16.6W×1.22 W=81.25°C

Compare to applying the RΘJC thermal resistance extracted from the JEDEC PCB which has less copper heat sink, no vias and thin copper traces extending from each IC pin, we obtain a TJ of 95.7°C as shown in Equation 42. The error in this result is mostly attributed to the PCB mismatch between the JEDEC PCB and the EVM as well as the thermal interface between the measured case temperature and die temperature.

Equation 42. TJ=TC+RΘJC×PD=61+28.5W×1.22 W=95.7

Finally, applying the RΘJA thermal resistance, also extracted from the JEDEC PCB, which has less copper heat sink, no vias and copper fingers extending from each IC pin, we obtain a TJ of 89.8°C as shown in Equation 43. This result also assumes the error between the JEDEC PCB and the EVM but does not rely on measured case temperature and more closely agrees with Equation 43.

Equation 43. TJ=TA+RΘJA×PD=26+52.3W×1.22 W=89.8