SPRADJ8 October   2024 AM3351 , AM3352 , AM3354 , AM3356 , AM3357 , AM3358 , AM3359 , AM4372 , AM4376 , AM4377 , AM4378 , AM4379 , AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM62A1-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62P , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442 , DP83822H , DP83822HF , DP83822I , DP83822IF , DP83826E , DP83826I , DP83848-EP , DP83848Q-Q1 , DP83867CR , DP83867CS , DP83867E , DP83867IR , DP83867IS , DP83TC812R-Q1 , DP83TC812S-Q1 , DP83TC813R-Q1 , DP83TC813S-Q1 , DP83TC814R-Q1 , DP83TC814S-Q1 , DP83TG720R-Q1 , DP83TG720S-Q1 , DP83TG721R-Q1 , DP83TG721S-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. Terminology
  5. Prerequisites
  6. Quick Initial Steps
  7. Debug Overview
  8. Network Driver Initialization Process
  9. Ethernet PHY Analysis
  10. Ethernet MAC Statistics Analysis
  11. How IPv4 Address is Obtained
  12. Follow the Packet
  13. 10Debug Network Topologies and Techniques
    1. 10.1 Direct Connection
    2. 10.2 Static IP Addresses
    3. 10.3 Setting Low Bit Rates
    4. 10.4 Beware When Connecting to a Switch
  14. 11Linux® Utilities Summary
  15. 12Checklist for Requesting Ethernet Support

Checklist for Requesting Ethernet Support

When posting an inquiry on the TI E2E™ forum (related to an Ethernet communication issue using a Linux OS on the DUT), answer the following questions or complete the requested steps in the initial post:

  1. What is the TI SDK version in use?
  2. What is the TI processor in use?
  3. Is the DUT a TI EVM or a custom board?
  4. What is the test topology?
  5. If using a custom board, attach the DTS file for the custom board; do not cut and paste the DTS contents as the DTS file can be very long creating difficulty for readers to parse
  6. Attach the console boot log of the DUT
  7. Attach the results of ethtool <interface name> and ethtool -S <interface name> for the interface with the issue
  8. Indicate that you have reviewed this application note