SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P , DRA76P , DRA77P
To summarize, a subtile is a subtle refinement of a tile whose purpose is to:
A subtile is defined as a 128-bit 2D block, and a tile as an array of eight lines of eight subtiles, as shown in Figure 17-16.
Figure 17-16 Tile GeometryIn any tile, the subtile Sx,y at column x (0 =< x < 8) and row y (0 =< y < 8) is found at an offset of 16.(x + 8.y) bytes from the base address of the related tile. Besides, this array organization of subtiles is common to each tiled mode. For instance, the subtile S0,1 is always located at an offset of 128 bytes (that is, 16.(0 + 8 x 1) ) from the base address of the related tile.
Figure 17-17 shows the subtile mapping.
Figure 17-17 Subtile Mapping