SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P , DRA76P , DRA77P
The requests (reads or writes) sent to the L3_MAIN interconnect are pipelined and arbitrated in a round-robin scheme. The default arbitration scheme must be modified by setting the priority attribute of each pipeline as defined in the following bits:
By default, all pipelines have the same priority (normal), which means all pipeline requests are treated in a round-robin order manner. If one or more pipelines require a higher number of requests going to the L3_MAIN interconnect, its priority can be moved up to high priority. In this case, the high-priority pipeline is granted access before any pipeline in normal priority. If more than one active pipeline is in high priority, the behavior is the same as all active pipelines in normal priority. Normal active pipelines are not treated until all high active pipelines are finished. The ARBITRATION bit cannot be modified during the entire frame.
This functionality balances the bandwidth of the pipeline depending on its constraint. It can be used to give higher priority to the pipelines with real-time constraints versus non-real-time pipelines. For example, pipelines associated with the LCD output in stall mode must have lower priority than pipelines associated with TV output.