DLPS249 December 2024 DLP991U
PRODUCTION DATA
Figure 6-1 DMD Thermal Test PointsMicromirror array temperature can be computed analytically from measurement points on the outside of the package, the package thermal resistance, the electrical power, and the illumination heat load. The relationship between micromirror array temperature and the reference ceramic temperature is provided by the following equations:
where
The electrical power dissipation of the DMD (QELECTRICAL) is variable and depends on the voltages, data rates and operating frequencies of each specific application system. QELECTRICAL should be measured in each specific application to determine the proper value of QELECTRICAL to use in the equations below. To calculate array temperature, the value for electrical power dissipation of the DMD (QELECTRICAL) used in the example calculations below is 6.2 Watts (Typ). The absorbed power from the illumination source is variable and depends on the operating state of the micromirrors and the intensity of the light source. The equations shown above are valid for each DMD chip in a system. It assumes an illumination distribution of 91.0% on the active array, and 9.0% on the array border.
Sample calculations for off-state and on-state are shown below.