Follow the instructions below for loading the DLPC964 Apps binary onto the FPGA via a bitstream using Vivado Lab Solutions 2018.2:
Note: Click the link above to download Vivado Lab Solutions 2018.2. Once the web page is loaded, find the archived 2018.2 folder and then navigate to the Vivado Lab Solutions 2018.2 downloadable link and download the installation.
Note: The FPGA needs to be reloaded each time power is lost or disconnected from the AMD EVM.
- Plug the Micro-B USB cable into the side of the VC707 and the other end into the computer running Vivado.
- Start Vivado Lab Solutions 2018.2 on the computer.
- Select Open Hardware Manager from the main window.
- Click open target located in the top left of the hardware manager then Auto Connect.
- If the AMD EVM is the only FPGA plugged into the computer, then Vivado automatically connects to the AMD EVM.
- Right-click on the FPGA and select Program Device.
- Navigate to the appstop.mcs file and select Program.