DLPC964 Version—Contains the build number and version information for the DLPC964 Firmware.
DLPC964 Temperature—Displays the temperature of the DMD in Celsius
DMD —DMD internal temperature
DMD Board—Surface temperature of physical DMD board
Main Status—Contains the status of the DLPC964 PLL Lock, DMD POWERGOOD, DMD High-Speed Interface, UBLAZE, and DMD Parked.
HSS Channel Status—Indicates the status of the Aurora 64B/66B inputs to the DLPC964 Controller.
PLL Lock
User PLL—When unchecked, the user clock is not lock. When checked, user clock is locked.
GT0 PLL—The source for the MMCM to generate the user clock and determines if the PLL is lock.
Hard Error—Indicates if the HSS requires a reset to recover from a hard error condition.
Channel Up—Determines if the Aurora Channels 0-3 are up and running.
HSS Soft Error Count—Contains the Aurora 64B/66B Channel 0-3 total soft error count.
HSS Lane Status Up—Indicates the status of each individual lane of the Aurora 64B/66B input to the DLPC964 Controller.
HSSI Lane Integrity Test Results—The Lane Integrity Test contains the testing results of DMD High Speed Serial Interface for Channels 0-3. Each lane for this interface (7:0) can be checked for passing results.
Note: If the Channels are not passing, this results in a DMD Interface D-Sync Error.