SBAA531 November 2021 ADS8860 , ADS8862 , ADS8881 , ADS9110 , ADS9224R
The bandwidth of the input circuit depends mainly on the sample and hold circuit. The input resistor Rsh and input capacitor Csh can be used to calculate the bandwidth. Some SAR ADC data sheets show a specified bandwidth that is slightly different from the bandwidth set by the input Rsh × Csh filter, but typically this difference is very small and can be neglected. The bandwidth of the ADC is very important in noise simulations as proper bandwidth modeling allows calculation of total noise. Figure 2-5 illustrates how the internal bandwidth is set by the sample and hold circuit.
Figure 2-5 Bandwidth of ADC