SBASAP7A December 2024 – April 2025 ADC3664-SP
PRODUCTION DATA
The ADC3664-SP includes an optional output scrambler feature in 2-wire mode only. The scrambler can enabled by enabling the DSP features (D2 of 0x24) and enabling scrambling (D6 of 0x22). When enabled, each sample is split into two halves. Each half of the samples stream is scrambled independently. For example, if the samples stream is at an 18-bit resolution, the stream is divided into two halves consisting of bits D17-D9 & D8-D0. The two halves are fed into independent scrambling blocks where each input bit (x[k]) of each scrambler is XOR-ed with 2 previous bits (y[k-14] and y[k-15]) as shown in Figure 7-11. Since this is a self-synchronizing scrambler, the start up state of the scrambler can be ignored.
For proper descrambling, the sample stream halves must be descrambled independently then the descrambled data can be used to reconstruct the samples. On the receiver side, the incoming serial data stream can be descrambled by XOR-ing each incoming bit (y[k]) with 2 previous bits (y[k-14] and y[k-15]).
For example, in 2-wire and 18-bit mode, one lane carries the odd bits (D17, D15, D13, etc.) and one lane carries the even bits (D16, D14, D12, etc.). When scrambling is enabled, the bit mapper needs to be configured so that one lane carries bits D9-D17 and the other lane carries D0-D8 (LSB first for each lane). An example data flow diagram of scrambling an 18-bit sample stream is shown in Figure 7-12, where D17:D0 is the sample provided by the ADC after the resolution select block, the sample is split into D0-D8 and D9-D17 and fed into each scrambler (LSB first) and S0-S17 are the resultant scrambled bits.