SBAU279 October 2020 ADS7038-Q1
The EVM and PAMboard should come packaged together. If they are not, for correct functionality, the boards need to be installed together properly.
To install the EVM to the PAMboard, stack the ADS7038Q1EVM board on the PAMBoard. Make sure the 20-pin connector (J1, J3) on the ADS7038Q1EVM is mapped to left connector on the PAMBoard, and the EVM connector (J4, J2) is mapped to right connector on the PAMBoard. The silk screen on the ADS7038-Q1 must match with the PAMBoard. Figure 3-1 shows the correct installation. The board headers must be flush. Make sure the USB is not plugged in during board connections. After matching the boards together, connect the PAMBoard micro USB data port to an available USB port on the PC.
Figure 3-1 ADS7038Q1EVM Lined up With PAMBoard.