SBAU416C November 2022 – March 2025
The Histogram tool represents the distribution of ADC output codes for a given sample set. The accuracy of the statistical summary can be improved by increasing number of samples, which increases the sample size at the cost of extra test time. Select the channel to measure and configure the number of samples, Vref, and ADC Full-scale. Then, press the GET HISTOGRAM button as shown in .
The cumulative effect of noise coupling to the ADC output comes from sources such as the input drive circuits, the reference drive circuit, the ADC power supply, and the ADC. The total noise is reflected in the standard deviation of the ADC output code histogram that is obtained by performing multiple conversions of a DC input applied to a given channel. Selecting the correct reference voltage gives the result in units of voltage instead of codes.