SBAU416C November 2022 – March 2025 ADS9813 , ADS9817
The INL and DNL tool measures the linearity of the of the ADS9813EVM by applying a full-scale, low-distortion sinusoidal input signal. The accuracy improves if the number of hits per code is increased at the cost of extra test time. Select the channel to measure and the hits per code. An input signal greater than full-scale is required to verify that all ADC codes are tested. An input signal of +0.1 dBFS is sufficient. Then press the GET INL/DNL button to run this tool as shown in Figure 3-13. Users can use the listed coherent sampling frequency for either the SMPL_CLK or the input signal for best INL and DNL performance.