SBAU417A July 2025 – September 2025 AFE7952
The Latte UI is split into eight windows (labeled 1 to 8) with the following functions:
This window (also called Scripts) shows the list of python scripts available that generate the register commands to configure the AFE7952EVM. The script files shown are located in the ..\Documents\TexasInstruments\AFE79xxLatte\projects\AFE79xx\bringup folder. Modify and create new scripts as necessary, which appear in the Window 1 sub-window when Latte restarts.
This window (also called Editor) shows the code in the script currently selected and can be used to modify and save the code as necessary.
These windows update as the scripts run to configure the AFE7952EVM and mostly are informational.
This window (also called Command Line) is used to enter and run individual commands. Examples of such commands include changing the TX, RX, and FBRX DSA, NCOs, and so forth.
This window (also called Log) displays messages during execution of scripts to display the current status. This window is also used for troubleshooting.