SBAU417A July 2025 – September 2025 AFE7952
TSW14J58EVM: On the LED strip, TX_Sync and RX_Sync is not illuminated. TX_Active and RX_Active is illuminated. Illumination specifications are necessary requirements for the JESD204B transceiver mode to work. TX_Active flashing indicating the TXDAC JESD204B link is established, while RX_Active flashing indicating the RXADC or FBADC JESD204B link is established.
AFE7952EVM: Enable data transmission on the DAC and data capture on the ADC. Adjust the RXNCO, FBNCO, and TXNCO at this point.
Adjust the RXDSA, FBDSA, and TXDSA at this point.
## Set RX DSA
afeInst = 0 #AFE Instance of AFE79_INST_TYPE type. If using the EVM this should be 0.
rxChSel = 0 #Value to select the RX chain.Value 0 for RXA to 3 for RXD.
dsaSetting = 20 #Analog DSA Index. Attenuation applied is dsaSetting*0.5dB
CAFE.setRxDsa(afeInst,rxChSel,dsaSetting)
## Set TX DSA
afeInst = 0 #AFE Instance of AFE79_INST_TYPE type. If using the EVM this should be 0.
txChSel = 0 #Value to select the TX chain.Value 0 for TXA to 3 for TXD.
dsaSetting = 20 #Analog DSA Index. Attenuation applied is dsaSetting*1dB
CAFE.setTxDsa(afeInst,txChSel,dsaSetting)