SBAU488 June   2025

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 Hardware Overview
    2. 2.2 Assembly Instructions
    3. 2.3 Interfaces
      1. 2.3.1 Analog Input
      2. 2.3.2 Isolated Amplifier (AMC3302) Analog Output
      3. 2.3.3 Isolated Comparator (AMC23C15) Analog Output
    4. 2.4 Power Requirements
      1. 2.4.1 VDD2 Input
    5. 2.5 Test Points
    6. 2.6 Lug Information
    7. 2.7 Best Practices
  9. 3Implementation Results
    1. 3.1 Evaluation Procedure
      1. 3.1.1 Equipment Setup
      2. 3.1.2 Test Procedure
      3. 3.1.3 Full Signal Chain Evaluation Procedure
    2. 3.2 Performance Data and Results
      1. 3.2.1 Shunt Selection Calculations
      2. 3.2.2 Filter Selection
  10. 4Hardware Design Files
    1. 4.1 Schematics
    2. 4.2 PCB Layouts
    3. 4.3 Bill of Materials (BOM)
  11. 5Additional Information
    1. 5.1 Trademarks
  12. 6Related Documentation

Full Signal Chain Evaluation Procedure

Note: Verify that the outputs of the connected supplies are disabled before connecting or disconnecting equipment.
  1. Set the 5V (±10%) source and limit the current to 50mA as noted above. Connect the EVM voltage source to the VDD pin of the connector, referenced to GND2. Turn on the power source and verify that there is no more than the specified current limit in the device data sheet drawn.
  2. Connect DMMs to the following test points. Refer to Figure 3-1, Figure 3-2, and Figure 2-1 for test procedure setup and connection mapping.
    1. High current power supply control shunt: VIN
    2. AMC3302 input, INP and INN: VINP/INN
    3. AMC3302 differential output, OUTP and OUTN: VOUT_DIFF
    4. AMC3302 single-ended output, OUT(SE) and GND: VOUT_SE
    5. AMC23C15 output, OUT1 (or OUT2), and GND: VOUT1
  3. Connect the high-current carrying cables to the positive and negative lugs, IN+ and IN–. For high-side measurement of positive current, IN– sources to the electronic load; for negative current, IN+ sources to the load. Set current bounds if supplies allow. Turn on all connected supplies.
  4. Apply the appropriate full-scale linear input sweep ±200A range. Incrementing 0.5A every 0.2s is appropriate for evaluation.
  5. Record the five DMM outputs for the entire full-scale linear input sweep.
  6. To evaluate the current sensing performance of the EVM, calculate the following errors across the entire current sweep. Equations i calculate the error at a given input current and equations ii calculate the error over a specified current range at a given input current. An example range is ±50A.
    1. Default Values:
      .         R IND = 4 . 9 kΩ
      .         I B = 36 μA
      .         GAIN AMC 3302 = 41
      .         V OFFSET = 2 . 5 V
      Shunt Resistor Error:
      .         i .   E SHUNT = V IN × R IND R IND + R 5 + R 8 + I B × R 20 - V INP / INN
      .         ii .   E SHUNT   % FS = E SHUNT E SHUNT ( I IN = - 200 A ) - E SHUNT ( I IN = 200 A ) × 100
    2. AMC3302 Error:
      .         i .   E AMC 3302 = V OUT_DIFF - V INP / INN × R IND R IND + R 5 + R 8 × GAIN AMC 3302
      .         ii .   E AMC 3302   % FS = E AMC 3302 E AMC 3302 ( I IN = - 200 A ) - E AMC 3302 ( I IN = 200 A ) × 100
    3. Differential to Single-Ended Error:
      .         i .   E DIFF → SE = V OUT_SE - V OUT_DIFF × R 4 R 7 + V OFFSET
      .         ii .   E DIFF → SE   % FS = E DIFF → SE E DIFF → SE ( I IN = - 200 A ) - E DIFF → SE ( I IN = 200 A ) × 100
    4. Total Error:
      .         i .   E TOTAL = V OUT_SE - V OFFSET +   ( V IN × R IND R IND + R 5 + R 8 + I B × R 20 ) × GAIN AMC 3302 × R 4 R 7
      .         ii .   E TOTAL   % FS = E TOTAL E TOTAL ( I IN = - 200 A ) - E TOTAL ( I IN = 200 A ) × 100
  7. Plot calculated results against input current, IIN. Results shown in Figure 3-3 are taken over temperature from two samples.
    AMC-AMP-200A-EVM AMC-AMP-200A-EVM Total
                            Error %FS Results Figure 3-3 AMC-AMP-200A-EVM Total Error %FS Results
  8. To evaluate the overcurrent detection performance, measure VOUT1 or VOUT2. By default, VOUT1 is low at IIN = ±288A or VIN = ±72mV ± 2.5mV and VOUT2 toggles at VIN =±60mV.
  9. Repeat these steps at hot and cold temperatures. Calibrate if necessary.