SBOA578A January   2025  – September 2026 TMCS1123 , TMCS1123-Q1 , TMCS1126 , TMCS1127 , TMCS1127-Q1 , TMCS1133 , TMCS1133-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Initial Examination of TMCS EVM With Corresponding Copper Lugs
    1. 2.1 Individual EVMs
    2. 2.2 Initial Examination of 3oz and 4oz Copper Single Panels
      1. 2.2.1 TMCS1123EVM 3oz and 4oz Single Panel
      2. 2.2.2 TMCS1143EVM 3oz and 4oz Single Panel
  6. 3Experimental Setup and Discussion
  7. 4Case 1: Copper Weight
    1. 4.1 TMCS1123EVM Varying Copper Weight
    2. 4.2 TMCS1143EVM Varying Copper Weight
  8. 5Case 2: Polygon Sizing
    1. 5.1 TMCS1123EVM Varying Polygon Sizing
    2. 5.2 TMCS1143EVM Varying Polygon Sizing
  9. 6Summary
  10. 7References
  11. 8Revision History

TMCS1123EVM Varying Copper Weight

The results for this section apply to the TMCS1123, TMCS1126, TMCS1127, and TMCS1133.

Figure 4-1 shows the typical footprint of the TMCS1123EVM.

 TMCS1123EVM PortionFigure 4-1 TMCS1123EVM Portion
Figure 4-2 examines the thermal results from each copper weight as current grows. As expected, the thicker the copper weight, the more current the board can handle.
 TMCS1123EVM Thermal Response Curves for all Copper WeightsFigure 4-2 TMCS1123EVM Thermal Response Curves for all Copper Weights
From the chart, the following observations can be made:
  • A doubling of copper results in roughly the same magnitude improvement, at least at lower thickness levels. From 1oz to 2oz, an approximate 10A improvement from 55A to 65A. At the 4oz mark, this moves to 75A capability, which is again a 10A improvement, for a doubling from 2oz to 4oz. However, also, the 6oz copper was capable of 85A, which by the same relationship can be expected of 8oz copper.
  • At higher copper levels, for example, beyond 4oz, we begin to see diminishing returns in capability. While 6oz is still an improvement over 5oz, and 5oz is an improvement over 4, these curves are much tighter in distribution, with some worst case devices matching best case performance of the next copper weight.
  • As stated previously, board manufacturing tolerances and capabilities can change the thermal profile from board to board. As an example, examining the 1oz data shows that at the point the worst performing device reaches 165°C, the best performing device is only at 145°C. As such, it is imperative that sufficient headroom be made in the design to make sure of success in the face of lot to lot variation