SBOSAN2A August 2025 – December 2025 PGA854
PRODUCTION DATA
The output voltages of the PGA854 are balanced with respect to the voltage on the output common-mode pin, VOCM. The starting point for most designs is to assign an output common-mode voltage for the PGA854. For ac-coupled signal paths, this voltage is often the default mid-supply voltage, so as to retain the most available output swing around the voltage centered at VOCM. For dc-coupled signal paths, and low voltage output supply, set this voltage between a maximum of VLVDD – 1.5V and minimum of VLVSS + 1.5V. for higher voltage supplies, set VOCM between VLVDD – 2V and minimum of VLVSS + 2V. Note that For precision ADC applications, this voltage is typically the input common-mode voltage of the ADC.
The voltage at the VOCM pin is internally buffered to bias the fully differential output amplifier, eliminating the need for an external VOCM buffer. In the event that the VOCM pin is left floating, the output common-mode control voltage is biased at output mid-supply using an internal 500kΩ-500kΩ resistor divider network connected between the output-stage power-supply pins.