SCPS286C July 2025 – October 2026 TPLD2001
PRODUCTION DATA
Combinational logic is supported via Look-up Tables (LUTs) within the TPLD2001. Inputs and outputs for the combination function macro-cells are configured from the connection mux with specific logic functions being defined by the state of OTP bits.
The TPLD2001 has fourteen configurable use logic blocks (macro-cells) that can serve as a combinational or sequential logic function. In each case, the macro-cells can serve as a Look-up Table (LUT), or as another logic or timing function. See the list below for the functions that can be implemented in these logic blocks: