SCPS286C July 2025 – October 2026 TPLD2001
PRODUCTION DATA
The following section provides the registers accessible in the TPLD2001.
Reads from and writes to the device are asynchronous; thus current counter count value may change by the time the read occurs depending on the speed of the clock used for the counter and of the serial communications interface.
When updating counter data, it is recommended to put the counter in reset. If counters are not kept in a reset state, updates to CNT0 to CNT5 will not take affect until the next reset; whereas updates to CNT6 to CNT9 will take immediate affect.
After updating the counter data, two clocks are required to re-initialize the counter. If an External Clock option is used, provide the two clocks for proper operation of the counter.