SDAA028 June 2025 MSPM0C1104 , MSPM0C1105 , MSPM0C1106 , MSPM0G1106 , MSPM0G1107 , MSPM0G1506 , MSPM0G1507 , MSPM0G1518 , MSPM0G1519 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3518 , MSPM0G3518-Q1 , MSPM0G3519 , MSPM0G3519-Q1 , MSPM0H3215 , MSPM0H3216 , MSPM0L1306
If the implementations above cannot be used in the application, then use GPIO to detect for 0% or 100% duty cycle high or low. This implementation needs an additional GPIO to detect PWM. The internal connection can be connected as shown in the demo code.
Figure 2-6 GPIO Implementation Connection in the
DemoAlthough IOMUX has the input mux module, TI recommends to use one GPIO as the capture input of the timer and the GPIO input for 0% or 100% duty cycle high or low. There can be one missing PWM cycle if there is a non-0% or non-100% duty cycle PWM when the IO mux stays in GPIO mode, and can also have some glitches when changing back to the capture mode of the timer. This implementation of using two GPIOs can avoid these issues.