SDAA062 September   2025 TMS320F28P559SJ-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Intelligent Cabin and IVI System
    2. 1.2 USB Interface Application in IVI
    3. 1.3 TMS320F28P55x Introduction
  5. 2USB Composite Device Enumeration and Data Report
    1. 2.1 USB Composite Device Enumeration
      1. 2.1.1 Descriptor Structure
      2. 2.1.2 Descriptor Types
        1. 2.1.2.1 Device Descriptor
        2. 2.1.2.2 Configuration Descriptor
        3. 2.1.2.3 Interface Descriptor
        4. 2.1.2.4 Endpoint Descriptor
        5. 2.1.2.5 String Descriptor
    2. 2.2 USB Composite Device HID Data Report
      1. 2.2.1 Data Report Item
      2. 2.2.2 HID Report Descriptor Structure
        1. 2.2.2.1 Main Item
        2. 2.2.2.2 Global Item
        3. 2.2.2.3 Local Item
    3. 2.3 Example of Building a HID Report Descriptor
  6. 3Software Realization
    1. 3.1 APIs for USB Composite Device Initialization
      1. 3.1.1 USBStackModeSet
      2. 3.1.2 USBDCDCCompositeInit
      3. 3.1.3 USBDHIDCustomCompositeInit
      4. 3.1.4 USBDCompositeInit
    2. 3.2 APIs for USB Composite Device CDC Data Report
      1. 3.2.1 USBBufferSpaceAvailable
      2. 3.2.2 USBBufferWrite
      3. 3.2.3 USBBufferRead
      4. 3.2.4 USBDCDCTxHandler
      5. 3.2.5 USBDCDCRxHandler
    3. 3.3 APIs for USB Composite Device HID Data Report
      1. 3.3.1 USBDHIDCustomTouchEvent
      2. 3.3.2 USBDHIDCustomReportKey
    4. 3.4 APIs for USB Composite Device Simulation
      1. 3.4.1 MultTouchSimHandler
      2. 3.4.2 KeySimHandler
    5. 3.5 APIs for USB Device Operate States Query
      1. 3.5.1 USBDCDCControlHandler
      2. 3.5.2 CustomHandler
  7. 4System Test
    1. 4.1 Test Setup
    2. 4.2 USB SCI CDC Device Function Test
    3. 4.3 USB Touch Screen HID Device Function Test
    4. 4.4 USB Button HID Device Function Test
  8. 5Summary
  9. 6References
  10. 7Appendix

USBBufferRead

This function reads up to ui32Length bytes of data received from the USB host into the supplied application buffer. If the receive buffer contains fewer than ui32Length bytes of data, the data that is present is copied and the return code indicates the actual number of bytes copied to pui8Data.

Table 3-7 USBBufferRead API Input Variables and Descriptions
Input Variables Description
psBuffer The pointer to the buffer instance from which data is to be read.
pui8Data The buffer into which the received data is written.
ui32Length The size of the buffer pointed to by pui8Data.