SDAA062 September 2025 TMS320F28P559SJ-Q1
To verify the button HID device function, users can see a new HID-compliant touch screen is added to human interface devices in the Window Device Manager, as shown in Figure 4-3. Users can see the 10 points movement in the screen if the PC screen can support touch function.
Figure 4-3 PC Device Manager View of USB
HID Touch Screen Devices