SDAA228 September 2026 MSPM33C321A
The BSL supports returning an application version number through the BSL interface. This support allows the BSL host to interrogate the firmware version without the ability to read the firmware. The version field address is 32-bits in length. Program the version value in the corresponding MAIN flash.
Use the APP_REV_POINTER field to set the address of the application version word. The version data only returns if the specified address corresponds to a valid flash memory address. If the given flash address is not programmed, then the ROM BSL returns 0h.