If the BCR configuration data fails the CRC check during boot, a catastrophic boot error results and the following limitations are imposed:
- The error cause is logged in the CFG-AP as a boot diagnostic
- The BSL is not invoked, even if the BSL was configured as enabled
- The user application is not started
- No application debug access is enabled
- A pending SWD factory reset command, if enabled or enabled with password, is honored
- A pending TI failure analysis flow entry, if enabled, is honored
- The boot process re-attempts up to three times
- If the 2nd or 3rd attempt
passes, the device boots normally
- If the 3rd attempt does
not pass, no further boot attempts are made until the next BOR or
POR