SDAA228 September 2026 MSPM33C321A
Other than the BSL configuration ID, there are a few more features that support customization using the SysConfig tool, as shown in Figure 4-12, including:
Whenever the BSL configuration changes, the SysConfig tool automatically calculates the CRC Checksum value, so the user only focuses on the customized BSL features and can easily generate the NONMAIN firmware files.