SDAA565 October 2026 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6422 , AM6441 , AM6442
The OSPI PSRAM from AP Memory is not available on the default TMDS64EVM, and is only available on the modified TMDS64EVM that follows the PROC101E1_OSPI schematic. The modification made to the default EVM is the addition of the TS3DDR3812RUAR high-speed switch that multiplexes the OSPI signals between the OSPI NOR Flash and OSPI PSRAM.
The OSPI_SW_SEL signal is driven by pin 23 of the TCA6424A I/O expander, which is controlled over I2C1. When the OSPI_SW_SEL is asserted (driven high), the OSPI signals are routed to the OSPI PSRAM, enabling the SoC to communicate with the OSPI PSRAM. By default, the OSPI_SW_SEL is low, so that the OSPI signals are routed to the OSPI NOR Flash, enabling the default boot from OSPI NOR Flash.
Figure 2-1 OSPI Signal Routing Through High-Speed
Switch