SFFS700 May 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
The Analog-to-Digital Converter (ADC) module is used to convert analog inputs into digital values. Results are stored in internal registers for later transfer by CLA, DMA or CPU. The C2000 MCU device family products implement up to four modules with shared channels used for fast conversion (ping-pong method).
The following tests can be applied as diagnostics for this module (to provide diagnostic coverage on a specific function):
The following tests can be applied as a test-for-diagnostic on this module: