SGLS154F November 2000 – September 2025 TLV3701-Q1 , TLV3702-Q1
PRODUCTION DATA
The TLV370x devices have two operating common-mode ranges: within-the-rail and over-the-rail.
Within-the-Rail Operation: IN+ and IN- are less than (V+)
When an input pin is operating less than (V+), there are two operating regions defined where input voltages can be compared: low common-mode and high-common mode. In low-common mode which extends typically from 0V to (V+) - 1V, the typical input bias current is less than 1pA. In high common-mode which extends typically from (V+) - 1V to (V+), the typical input bias current is less than 14nA.
Over-the-Rail Operation: IN+ and/or IN- are greater than (V+)
The TLV370x devices have a distinctive input stage that allows the input common mode range to extend from 0V to 16V independent of the supply voltage. This feature means that operation at low supply voltages does not limit the range of input voltages that can be compared. When an input pin is operating over-the-rail (above (V+)), the bias current increases to a typical value of 55nA.