SLAAE29B January 2023 – August 2026 MSPM0C1105 , MSPM0C1106 , MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1218 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1518 , MSPM0G1519 , MSPM0G3105 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3218-Q1 , MSPM0G3505 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3518 , MSPM0G3518-Q1 , MSPM0G3519 , MSPM0G3519-Q1 , MSPM0L1105 , MSPM0L1106 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
MSPM0 devices contain an immutable root-of-trust boot configuration routine contained in read-only memory (ROM). The boot configuration routine (BCR) is always the first code to run on the Cortex-M0+ processor following a BOOTRST of the device. The BCR also runs upon software invocation of the bootstrap loader (BSL) as it is needed for authorizing the BSL entry. The core responsibilities of the BCR are to:
Load the user-specified device configuration (including the security policies) from the NONMAIN flash memory region into logic, and verify the integrity of the user configuration data through CRC-32
Determine whether to release the AHP-AP, ET-AP, and PWR-AP DAPs at the end of the BCR, after the CSC issues INITDONE (discussed in detail in Section FIX), or never.
Log any boot errors to the CFG-AP