SLCA006 June 2025 LM339 , LM393 , LMH7322 , TL331 , TLV1812 , TLV1871 , TLV1872 , TLV3601 , TLV3604
The differential push-pull out is a comparator with two identical Push-Pull outputs, where one output is inverted 180° from the other and swing close to the supply rails. Because the inversion is done internally from a common node, there is minimal skewing (delay) between the two outputs that can be caused by using an external inverter logic gate.
The differential outputs can be used to create a differential transmission scheme, or, as two single outputs 180° apart to drive loads such as H bridge transistors or MOSFETs.
Devices that support this standard are the TL3016, TL3116, TL712 and TL714.
| Advantages | Disadvantages |
|---|---|
|
|