SLLA661 April 2025 MCF8315A , MCF8315C , MCF8315C-Q1 , MCF8315D , MCF8316A , MCF8316C-Q1 , MCF8316D , MCF8329A , MCF8329A-Q1
| Sl No | Requirements |
|---|---|
| 1 | Laptop installed with MOTORSTUDIO |
| 2 | .json file (refer this e2e FAQ for .json files) |
| 3 | MCF8329A/16A/16C/16D/15A/15C/15D EVM |
| 4 | BLDC Motor |
| 5 | DC power supply |
| 6 | USB Cable |
| 7 | Connecting wires |
Table 2-2 are the required parameters specific to the motor that the user needs to note down before starting next steps
| Sl No | Required Parameters |
|---|---|
| 1 | Rated input DC voltage (V) |
| 2 | Maximum motor speed (RPM/Hz) |
| 3 | Rated motor phase peak current (A) |