SLLA661 April 2025 MCF8315A , MCF8315C , MCF8315C-Q1 , MCF8315D , MCF8316A , MCF8316C-Q1 , MCF8316D , MCF8329A , MCF8329A-Q1
In manual measurements, use lab equipment and motor data sheet to identify the motor parameters as mentioned in Table 3-2.
| Manual Measurements | How to Measure |
|---|---|
| Motor phase resistance | Using the instructions in the Motor Parameters FAQ measure the phase resistance and inductance along with the BEMF constant of the motor |
| Motor phase inductance | |
| Motor BEMF constant | |
| BASE_CURRENT (applicable for MCF8329A only) | This register setting depends on the shunt resistor used on the board. Refer the MCF8329A Tuning Guide for calculating BASE_CURRENT |
| Rated speed of the motor (MAX_SPEED) | The maximum rated speed of the 3-phase BLDC motor (in Hz). Typically found in the data sheet of the motor. If the mechanical speed is in RPM (N) convert the value to electrical frequency (f in Hz) using the formula: f = P x N / 120. P is the number of rotor poles |
| Rated current of the motor |
The rated peak phase current value for the 3-phase BLDC motor when this is driven at rated speed and rated voltage with load. Typically found in the data sheet of the motor. |