SLLA684 June   2025 MCF8315A , MCF8315C , MCF8315C-Q1 , MCF8315D , MCF8316A , MCF8316D

 

  1.   1
  2.   Summary
  3. 1Profile
    1. 1.1 Profile of MCF831x
    2. 1.2 Burning challenges
  4. 2Burning tool based on LP-MSPM0G3519 evaluation board
    1. 2.1 Profile of MSPM0G351x
    2. 2.2 Introduction of LP-MSPM0G3519 evaluation board
    3. 2.3 LP-MSPM0G3519 evaluation board burning tool hardware requirements and features
      1. 2.3.1 Burning platform hardware requirements
      2. 2.3.2 Burning tool function
  5. 3Procedure for using the burning tool
    1. 3.1 Hardware platform setup
    2. 3.2 Software Setup
      1. 3.2.1 Download and burn the firmware to LP-MSPM0G3519 using Uniflash
      2. 3.2.2 Import MCF831x json configuration file to the burning platform
    3. 3.3 Offline burning
  6. 4Summary
  7. 5References

Offline burning

After completing the hardware setup as described above, you can proceed to the burning stage.

 Burning connection diagramFigure 3-10 Burning connection diagram

After pressing LP-MSPM0G3519 evaluation board reset button, the following information appears in sscom with the blue LED remaining steadily lit.

 *****************************************************************
MCF8315 EEPROM Programming
SW Version: 2024-12-12
 *****************************************************************

Check MCF8315 I2C Address 
Current MCF8315 I2C Address is: 0x0 
Reading out MCF8315 EEPROM contents

Reg: 0x80 = 0x5c26cc84
Reg: 0x82 = 0xa8200000
Reg: 0x84 = 0x44c6c3a0
Reg: 0x86 = 0x9aa92334
Reg: 0x88 = 0xe29b1bd
Reg: 0x8a = 0xa50eccc3
Reg: 0x8c = 0x23800005
Reg: 0x8e = 0x16d2c546
Reg: 0x90 = 0x2dda0326
Reg: 0x92 = 0x7fd252d8
Reg: 0x94 = 0x2100a1a3
Reg: 0x96 = 0x21a80cfc
Reg: 0x98 = 0x7ffffff8
Reg: 0x9a = 0x80383d3d
Reg: 0x9c = 0x313fffc0
Reg: 0x9e = 0x7fff8000
Reg: 0xa0 = 0x3020f0
Reg: 0xa2 = 0x201
Reg: 0xa4 = 0x8000001
Reg: 0xa6 = 0x1
Reg: 0xa8 = 0x1f4f000
Reg: 0xaa = 0x2680200
Reg: 0xac = 0xc000104
Reg: 0xae = 0x1120000

Reading MCU Flash Contents for EEPROM Programming 
 
0x5c26cc84
0xa8200000
0x44c6c3a0
0x9aa92334
0xe29b1bd
0xa50eccc3
0x23800005
0x16d2c546
0x2dda0326
0x7fd252d8
0x2100a1a3
0x21a80cfc
0x7ffffff8
0x80383d3d
0x313fffc0
0x7fff8000
0x3020f0
0x201
0x8000001
0x1
0x1f4f000
0x2680200
0xc000104
0x1120000
 
Waiting for Button pressed to write EEPROM

Simply press S2 button on LP-MSPM0G3519 evaluation board to enter the download process. The blue LED blinks during the download process and the green LED blinks rapidly when the download is complete, indicating a successful burning. If a flashing red LED appears, it indicates that the burning fails and then a failure indication occurs in sscom.

 A prompt when burning and verification are completeFigure 3-11 A prompt when burning and verification are complete

MCU will automatically check the contents of the EEPROM in the MCF831x after the burning is complete, so as to ensure that the burning is correct and consistent.

If you need to download a new json file to the LP-MSPM0G3519 evaluation board, just keep pressing S2 button and press the Reset button again, and then sscom will prompt you to enter json file download mode and the user can download the new json file.