SLLA684 June 2025 MCF8315A , MCF8315C , MCF8315C-Q1 , MCF8315D , MCF8316A , MCF8316D
In order to import MCF831x json configuration file into the LP-MSPM0G3519 evaluation board, we need to use serial port software sscom, which is available at this address for this free software. http://www.daxia.com/download/sscom.rar
After connecting the LP-MSPM0G3519 evaluation board to the PC end using a micro USB, the serial port information can be seen in the device manager. Note that XDS110 Class Application/User UART (In COMxx, xx represents the actual number displayed by the user's computer) is used.
Figure 3-5 View port information of LP-MSPM0G3519 in WindowsOpen sscom software and select the corresponding COMxx port in the ComNumber drop down menu and 115200 baud rate. Click OpenCom button, press S3 Reset button on LP-MSPM0G3519 evaluation board, and sscom will output the following information. We can see the release date of the software version.
Since no json configuration file is stored internally in MSPM0G3519, it will default to json file download mode, waiting for the user to initiate json file download operation.
Figure 3-6 Burning tool output information interfaceClick OpenFile button to select json file to download. When opened, the window displays the contents of the current json file. Click the Send button to start json file download process.
Figure 3-7 Select json file in sscom
Figure 3-8 Burn json file in sscom
Figure 3-9 Json file burning success informationUpon successful burning of json file, the display will appear as shown in the diagram, and json file is checked automatically during this process to ensure that the burning is accurate. This is where all the preparation is done, proceeding to MCF831x burning phase.