SLLSFO4D December 2022 – August 2025 ISOM8710 , ISOM8711
PRODMIX
The input of ISOM871x can be driven by an inverting buffer or non-inverting buffer to change the truth table of the ISOM871x or provide sufficient input forward current to drive the device. Using a buffer is optional. If a buffer is used, the equation for RIN remains the same as shown above.
Sizing RIN based on the output voltage of the buffer, VBUF, and the desired forward input current, IF, Equation 1 becomes:
For example, using a buffer with a 5V output, and a desired IF of 5mA, RIN is calculated as: