SLOS196B October 1987 – June 2025 TLV2711
PRODUCTION DATA
The TLV2711 is designed to drive larger capacitive loads than most CMOS operational amplifiers. Figure 5-31 illustrate the ability to drive loads up to 600 pF while maintaining good phase margins (Rnull = 0 Ω).
A smaller series resistor (Rnull) at the output of the device (see Figure 6-1) improves the gain and phase margins when driving large capacitive loads. The addition of this series resistor has two effects. The first effect is that the series resistor adds a zero to the transfer function. The second effect is that the series resistor reduces the frequency of the pole associated with the output load in the transfer function.
The zero introduced to the transfer function is equal to the series resistance times the load capacitance. To calculate the improvement in phase margin, use Equation 1.
where
Figure 6-1 Series-Resistance Circuit