SLOS887G September 2014 – May 2025 TMP112-Q1 , TMP112D-Q1
PRODUCTION DATA
The default mode of the TMP112-Q1/TMP112D-Q1 device is continuous conversion mode. During continuous-conversion mode, the ADC performs continuous temperature conversions and stores each results to the temperature register, overwriting the result from the previous conversion. The conversion rate bits, CR1 and CR0, configure the TMP112-Q1/TMP112D-Q1 device for conversion rates of 0.25Hz, 1Hz, 4Hz, or 8Hz. The default rate is 4Hz. The TMP112-Q1 device has a typical conversion time of 26ms while TMP112D-Q1 has a typical conversion time of 10ms. To achieve different conversion rates, the TMP112-Q1/TMP112D-Q1 device makes a conversion and then powers down and waits for the appropriate delay set by CR1 and CR0. Table 7-5 lists the settings for CR1 and CR0.
| CR1 | CR0 | CONVERSION RATE |
|---|---|---|
| 0 | 0 | 0.25Hz |
| 0 | 1 | 1Hz |
| 1 | 0 | 4Hz (default) |
| 1 | 1 | 8Hz |
After a power up or general-call reset, the TMP112-Q1/TMP112D-Q1 device immediately begins a conversion as shown in Figure 7-7. The first result is available after 26ms (typical) for TMP112-Q1 and 10ms (typical) for TMP112D-Q1. The active quiescent current during conversion is 40μA (typical at 27°C) for TMP112-Q1 and 55μA (typical at 27°C) for TMP112D-Q1. The quiescent current during delay is 2.2μA (typical at 27°C) for TMP112-Q1 and 2.6μA (typical at 27°C) for TMP112D-Q1.