SLUSC25B February 2015 – October 2026 TPS2388
PRODUCTION DATA
COMMAND = 23h with 1 Data Byte, Write Only
Used to do a port(s) turn on during semiauto mode. This command is ignored if in manual mode. Note that if at completion of this command the addressed port is not turned on, the corresponding bits in the Detect/Class Enable register (register 14h) are being set, which means that detection and classification are performed continuously, as long as the class and detect enable bits are kept set.
Writing a 1 at a TmPONn bit will turn on the associated port but only if the IEEE802.3 TPON timing specification can be met. TPON specification is the time from the completion of a valid detection cycle to port turn ON.
If TPON specification cannot be met, a new detection cycle is restarted, followed by a classification cycle, at the end of which the port is turned on, but only if a valid detection and classification is returned. For this case, there is no additional attempt to turn on the port until this push button is reasserted.
Note that a port turn on will be performed only after both its current detection and classification cycle are completed
Note that writing a 1 at T1PONn and T2PONn of same port during the same write operation is interpreted as a T1PONn.
The corresponding PGCn and PECn bits of Power Event register will also be set depending on the result, while the CLSCn and DETCn bits of Detection Event register will be set based on the result and the CLCHE and DECHE bits in the General Mask register.
Also note that tOVLD, tLIM, tSTART, and disconnect events are prioritary over the power on command. During tOVLD, tLIM, or tSTART cool down cycle, any port turn on using IEEE Power Enable command will be ignored and the port will be kept off.
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Type 2 IEEE Power Enable Pushbutton | Type 1 IEEE Power Enable Pushbutton | ||||||
| T2PON4 | T2PON3 | T2PON2 | T2PON1 | T1PON4 | T1PON3 | T1PON2 | T1PON1 |
| W-0 | W-0 | W-0 | W-0 | W-0 | W-0 | W-0 | W-0 |
| LEGEND: R/W = Read/Write; R = Read only; W = Write only; -n = value after reset |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7–4 | T2PON4T2PON1 | W | 0 | If class 4 is detected during the first event classification, a second event classification is performed. If the last detection result is not valid or last classification result yields “over current” or is different from the first classification event result, the port is not turned on, and the STRTn bit in Start/Ilim Event register is set, while the corresponding fault code in the Power-on Fault register is written.
When power-on is complete and if class 4 has been detected, the corresponding PoEPn bit in PoE Plus register is set and the value of the corresponding Police Configuration register is set to 640mA (08h code). This is done within 5ms of completion of inrush. |
| 3–0 | T1PON4T1PON1 | W | 0 | Indicates only a single-event classification is performed, even if a class 4 PD is detected.
If the last detection result is not valid or last classification result yields “over current”, the port is not turned on, and the STRTn bit in Start/Ilim Event register is set, while the corresponding fault code in the Power-on Fault register is written. |