SLUSC82B April 2017 – July 2026 UCC24630
PRODUCTION DATA
The GND pin is the power and signal ground connection for the controller. The effectiveness of the filter capacitors on the signal pins depends upon the integrity of the ground return. Place all decoupling capacitors as close as possible to the device pins with short traces. The device ground and power ground should meet at the output bulk capacitor’s return. Try to verify that high frequency/high current from the power stage does not go through the signal ground.