SLUUCC4A October 2020 – September 2021 TPS92520-Q1
This section shows the detailed instructions for checking if there is an update and how to install it. Run the TPS92518, 520, 682 LaunchPad Evaluation Software and go to the Help menu, see Figure 5-20.
Figure 5-20 Help Menu and Checking for UpdatesClick Check for Updates > to run updater.
Figure 5-21 Update Screen 1Click Yes > to accept risks for accessing the Internet.
Figure 5-22 Update Screen 2Go to the LEDMCUEVM-132 (PSIL-132) and locate J15 and RESET_SW1. Install shorting jumper at J15 locations as seen and then press the RESET_SW1 as seen in Figure 5-23. This action places the MCU in Bootloader mode.
Figure 5-23 J15 Jumper and RESET_SW1 Switch for Bootloader ModeClick Yes > to run the updater. The LPP Updater will run and once finished will ask if you would like to re-launch the GUI applications.
Figure 5-24 Setup Screen 5Click Yes > to re-launch GUI.
A window appears indicating the the LEDMCUEVM-132 must be changed from bootloader mode to normal mode. This is accomplished by removing the shorting jumper from J15 then pressing the "RESET_SW1" switch and wait 3 seconds to ensure device drivers reload, see Figure 5-26.
Figure 5-25 Setup Screen 6
Figure 5-26 15 Jumper and RESET_SW1 Switch for Normal ModeClick the OK > button to restart the GUI.