SLUUCC4A October 2020 – September 2021 TPS92520-Q1
This section shows the detailed installation instructions with screen shots.
Figure 5-1 Setup Screen 1Click Next > to install.
Figure 5-2 Setup Screen 2Click Next > to accept the License Agreement.
Figure 5-3 Setup Screen 3Select Full Install and click Next > to install the evaluation software, the UniFlash, and the required XDS drivers. Full installation for both Windows 10 and 7 are provided.
Figure 5-4 Setup Screen 4If .NET Framework 4.5 or higher does not exist on the computer, the .NET Framework installation begins. Installation of .NET Framework will take several minutes. If .NET Framework 4.5 or higher exists on the computer, the installation jumps to the XDS driver installation.
Figure 5-5 Setup Screen 5A window appears indicating the completion of the .NET Framework installation.
Figure 5-6 Setup Screen 6Click next to proceed.
Figure 5-7 Setup Screen 7Click the Next > button to install the XDS driver.
Figure 5-8 Setup Screen 8The completion of the XDS driver installation is shown in Figure 5-8.
The TI-Emulators installation starts at this point. This will install the necessary drivers for running the application. In the next few steps as shown in Figure 5-9, Figure 5-10 and Figure 5-11 click Next > to perform the installation.
Figure 5-9 Setup Screen 9
Figure 5-10 Setup Screen 10Accept the license agreement in Figure 5-10.
Figure 5-11 Setup Screen 11In the next few windows click Next >, and if prompted by Windows Security about software installation as shown in Figure 5-12, select Install.
Figure 5-12 Setup Screen 12
Figure 5-13 Setup Screen 13The screen showing the completion of the TI Emulators installation is shown in Figure 5-13. Click on Finish to move to the next step.
The UniFlash installation starts at this point. UniFlash is required to program the LaunchPad. In the next few steps as shown in Figure 5-14, Figure 5-15 and Figure 5-16 click Next > to proceed and start the installation.
Figure 5-14 Setup Screen 14
Figure 5-15 Setup Screen 15
Figure 5-16 Setup Screen 16
Figure 5-17 Setup Screen 17When UniFlash installation is complete, click Finish to launch the UniFlash and program the LaunchPad.
Figure 5-18 Setup Screen 18Figure 5-18 shows the completion of the TPS92520-Q1 Evaluation Software . Un-check the Launch Application and click Finish.