SLUUD32A June 2024 – April 2025
Dynamic load (IT-DZT) applications require a specific Chemistry ID different from the standard IT Chemistry ID. If TI has already created a Chemistry ID and it has High Frequency data (Turbo Mode), TI can use the high frequency data to create the IT-DZT ID.
If this has not been done, the user must contact their local Field Applications Engineer (FAE) to ship cells in to be characterized and formatted into a Chemistry ID.
All IT-DZT profiles will be added to the chemistry settings once user programs the IT-DZT-ChemID. User still needs to ensure that DZT Critical Parameters are configured properly.