SLVAFZ1 May 2025 TPS25751 , TPS26750
The Vendor Information File (VIF) defines the capabilities of the end product which testers use to determine the applicable procedures and tests required to achieve USB Type-C and PD certification. Typically, the VIF is configured manually in the USB-IF recommended VIF Editor Tool.
TI's Application Customization Tool simplifies VIF generation by automatically generating a VIF based on the user's configuration. The generated VIF requires minimal changes, reducing common compliance failures related to manual entry of the VIF fields.
To generate a VIF using TI's Application Customization Tool, click on the Export drop-down button on the top-right side of the tool and click on Generate VIF file. This automatically downloads a file in .XML format to the default save directory on the user's computer. Refer to Figure 2-1.